The IEC operator yields the sine value of a number.
Permitted data types for input variables that measure the angle in radians: any numeric basic data type
Permitted data types for output variable: REAL
and LREAL
The permitted range for the input value is −2 to +2. On x86 and x64 systems: If the input value is outside of the permitted range, the function returns the input value.
Examples
Result in q
: 0.479426
.
ST
q := SIN (0.5);
FBD