The IEC operator yields the base-10 logarithm of a number.
The input variable can be any numeric basic data type, but the output variable must
be the data type REAL
or LREAL
.
Examples
Result in q
: 2.49762
ST
q := LOG(314.5);
FBD