The IEC operator is used for the "less than or equal to" function.
Permitted data types of the operands: any basic data type
If the first operand is less than or equal to the second operand, then the operator
yields the result TRUE
; otherwise FALSE
.
Examples
Result in Var1
: TRUE
ST
Var1 := 20 <= 30;