The IEC operator is used for the "greater than or equal to" function.
Permitted data types of the operands: any basic data type
If the first operand is greater than or equal to the second operand, then the operator
yields the result TRUE
; otherwise FALSE
.
Examples
Result: TRUE
ST
VAR1 := 60 >= 40;
FBD