View license informationPermalink

To view the license information of AC500 V3 products:

  1. In the Automation Builder device tree, double-click the PLC node.

    The PLC tab is opens.

  2. In the PLC tab, select “License Information”.

    Lic_View_PLC

    The project is scanned for required licenses.

    If you are logged into a PLC, the licenses available on the PLC are displayed.

    Missing required licenses are highlighted.