Installation manager provides a guided uninstallation procedure for Automation Builder and all related packages such as Mint Plug-in, Automation Builder Extensions, Drive Manager etc.
-
In the installation manager, select [Uninstall all].
-
If Automation Builder instances are running, a warning message is displayed.
Close active instances and select [Retry].
Select [Abort] to stop uninstalling the current package and continue with the next one.
Select [Ignore] to force uninstallation. This option is not recommended because it may lead to an incomplete uninstallation.
-
If the installation manager was launched from “Tools Installation Manager”, the following message is displayed as Automation Builder is still running:
Select [Yes] to close Automation Builder and continue.
With [No] to stop uninstalling the current package and continue with the next one.
-
The system may prompt to continue uninstallation for individual packages.
-
Successfully uninstalled components are indicated by the success icon
. Errors during uninstallation are indicated by the error icon and abort the process
. Errors during uninstallation are indicated by the error icon and abort the process.
Select “Show Log”, save the log data and send it to ABB support. Select [Finish] to complete the wizard.