TIME_TO/TIME_OF_DAY conversionsPermalink

Converting from the variable type TIME or TIME_OF_DAY to a different type:

The time will be stored internally in a DWORD in milliseconds (beginning with 12:00 A.M. for the TIME_OF_DAY variable). This value will then be converted.

When you perform a type conversion from a larger to a smaller type, you risk losing some information.

For the STRING type variable, the result is a time constant.

Examples in ST:

(* Result is T#12ms *)
#str :=TIME_TO_STRING(T#12ms);

(* Result is 300000 *)
dw:=TIME_TO_DWORD(T#5m);

(* Result is 12 *)
si:=TOD_TO_SINT(TOD#00:00:00.012);

Examples in FBD:

time_to_string
time_to_dword
tod_to_sint