Structure DIAG_TXT_TYPEPermalink

This data type specifies the format of all kinds of diagnosis messages in textual format. It consists of a single string containing all details of a diagnosis message.

Name

Type

Initial

Comment

szDiag

STRING(512)

""

Diagnosis message as text, max. 512 characters

The text consists of the following data, separated by semicolon:

  • Timestamp in Date_And_Time (DT) format of eDiagEvent_Occured and added milliseconds

  • Error severity

  • Device name (max. 80 characters) as defined in Automation Builder device tree

  • The error text itself, composed of the interpretation of dwSubSysteminfo and dwAdditional and the error text plus remedy (if available) from Automation Builder text list according dwErrorCode. Displayed as: error text -> remedy.

Example

Battery empty or missing.

Battery_Empty_or_Missing