The following basic options and settings for user accounts can be configured:
-
“Maximum number of authentication trials”: If activated, the user account becomes invalid after the specified number of failed login attempts. If not activated, the number of failed attempts is unlimited. Default: option activated, number of trials: 3; Permissible values: 1-10.
-
“Automatically log out after time of inactivity”: If activated, the user account is logged out automatically after the specified period without keyboard or mouse input. Default: option activated, time: 10 minutes; Permissible time values: 1-180 minutes.
-
“New hash format for passwords”: If activated, account security is increased. When logging in for the first time, the stored password hash is converted. The new password hashes are not backward compatible.