Symbol:
Function: The command starts the static analysis for the active application and displays the results in the message view.
Call: Menu bar: “Build Static Analysis”
During the code analysis, CODESYS generates code just like the “Build Generate Code” command. The results of the analysis are displayed as errors and warnings
in the message view (“Build” category). The numbers refer to the corresponding rules as they are defined in the
project settings. The syntax for the displayed messages is “SA<rule number:<rule text>”.
See also