With this command it is possible to open and display the instance of the function block which is selected in the Object Organizer. In the same manner, a double click on the function block in the Object Organizer gives access to a selection dialog in which the instances of the function block as well as the implementation are listed. Select here the desired instance or the implementation and confirm using OK. The desired item is then displayed in a window.
If you want to view instances, you first have to log in! (The project has been compiled with no errors and downloaded to the PLC with 'Online' 'Login').