Automation Builder projects can be stored in Subversion (SVN) repositories by using the Project Version Control. The Project Version Control can be used to track changes on a project and to have access to historic versions of the whole project or objects in the project. It is possible to hold different versions of a project in branches and to compare these versions. The Project Version Control enables multiple engineers to work collaboratively on the same project.