'Project' 'Import'Permalink

In the resulting dialog box for opening files select the desired export file.

⮫ “'Project' 'Export'”

The data is imported into the current project. If an object with the same name already exists in the same project, then a dialog box appears with the question "Do you want to replace it?": If you answer Yes, then the object in the project is replaced by the object from the import file. If you answer No, then the name of the new objects receives as a supplement an underline and a digit ("_0", "_1", ..). With Yes, all or No, all this is carried out for all objects.

If the information is imported to link with a library, the library will be loaded and appended to the end of the list in the library manager. If the library was already loaded into the project, it will not be reloaded. If, however, the export file that is being imported shows a different storage time for the library, the library name is marked with a "*" in the library manager (e.g. standard.lib*30.3.99 11:30:14), similar to the loading of a project. If the library can not be found, then an information dialog appears: "Cannot find library {<path>\}<name> <date> <time>", as when a project is loaded.

In the message window the import is registered.