Question |
Answer |
---|---|
When a PROFINET Device or a Module is marked red (error), does that affect other devices or modules? |
No. They are not affected during a data exchange. |
Is a diagnosis in the field device is deleted when I reset or restart the application? |
This varies: Hardware problems are not solved by this, but errors by an incorrect parameterization are. |
Can a controller delete or confirm the diagnosis of the PROFINET Device? |
No, the PROFINET Device manages the diagnosis entries and sets the status of the modules. The PROFINET Controller merely confirms the receipt of incoming alarms at the log level. |