Object: PROFINET Controller
This tab is used to configure the media redundancy protocol (MRP) for the PROFINET Devices addressed by this PROFINET Controller.
|
“Enable” |
|
|
“MRP domain” |
Name of the MRP ring configuration |
|
“Device” |
Name of the device in the device tree or the name of the respective function block |
|
“Station name” |
The station name of the device |
|
“MRP instance” |
Index of the MRP ring (assigned automatically). Some devices support the participation in multiple MRP domains. |
|
“MRP role” |
Role of the device in the MRP ring
|
|
“Ring Port 1” “Ring Port 2” |
Ports of the ring that are part of the MRP ring. The neighboring port is displayed in brackets. |
For more information, see: ⮫ “Media Redundancy (MRP) ”
: Activates the MRP domain