This dialog is part of the option settings for the project data base ('Project' 'Options' 'Project source control'). Here you define how the objects of category 'Compile files' will be handled in the data base. (Besides that two further dialogs are available to define this for objects of category 'Project objects' and 'Shared objects'.)
For the input fields TCP/IP-Address, Port, Project name, see the description of dialog Project objects/Shared objects.
|
Create ASCII-symbol information (.sym) Create binary symbol information (.sdb) |
If this option is activated, then whenever a symbol file *.sym (text format) resp. *.sdb (binary format) will be created, this file will be written to the data base automatically. The entries in the symbol file are created like defined in the Project options category 'Symbol configuration'. |
|
Create boot project |
If this option is activated, then whenever a boot project will be created, this file will be written to the data base automatically . |
If you do a primary configuration, the configuration dialogs will appear one after the other, guided by a wizard (button Next). The settings made in the first dialog will automatically be inherited to the other ones. So those just have to be edited if modificiations are necessary.
Cancel will close the dialog without saving the done modifications in the currently opened dialog (the settings made in the previous dialogs will be kept anyway). You return to the main dialog 'Options' 'Project source control'.
If an already existing configuration has been modified, then the new settings (for all three dialogs) can be saved by pressing OK. After that the dialog will be closed and you return to the main dialog 'Options' 'Project source control'.
The settings will be stored in the project.