'Online' 'Step over'Permalink

symbol_onl_einzueber (AC500-S PT)

Shortcut: <F10>

This command causes a single step to execute. If a POU is called, the program stops after its execution.

⮫ “Single step”

If the present instruction is the call-up of a function or of a function block, then the function or function block will be executed completely. Use the 'Online' 'Step in' command, in order to move to the first instruction of a called function or function block.

⮫ “'Online' 'Step in'”

If the last instruction has been reached, then the program will go on to the next instruction in the POU.