'Online' 'Load file from PLC'Permalink

With this command, you can retrieve a file previously loaded into the controller using 'Online' 'Write file to PLC'. You receive the 'Load file from controller' dialog. Under Filename, provide the name of the desired file, and in the selection window enter the directory on your computer into which it is to be loaded as soon as the dialog is closed with the "Save" button.

⮫ “'Online' 'Write file to PLC'”