Depending on the processor module used, several configurations are possible for the onboard I/Os mostly different per group of channels.
|
Functionality to be realized |
Processor module type |
Digital input channels |
Configuration of the channel to be selected in Automation Builder |
Dedicated function block to be used in the user program |
Comments |
|---|---|---|---|---|---|
|
Digital inputs |
PM5012-x-ETH |
I0 … I3 |
Input/Interrupt |
Not needed |
Input delay can be sometimes configured according to channels type |
|
I4 ... I5 |
Input |
||||
|
PM5032-x-ETH, PM5052-x-ETH, PM5072-T-2ETH(W) PM5082-T-2ETH |
I0 … I3 |
Input/Interrupt |
Not needed |
Input delay can be sometimes configured according to channels type, for the PLC with relay outputs, the digital configurable channels have some other configurable features. |
|
|
I4 … I7 |
Input |
||||
|
I8 ... I11 |
Always inputs, not configurable |
||||
|
C12 … C13 |
Input/Output |