Mounting and demounting on DIN rail
Mounting with screws
If the terminal base should be mounted with screws, wall mounting accessories TA526 must be inserted at the rear side first ⮫ “TA526 - Wall mounting accessory”. These plastic parts prevent bending of the terminal base while screwing on.
|
Terminal base |
Number of TA526 wall mounting accessories |
|---|---|
|
TB560x TB561x |
1 |
|
TB562x TB564x TB566x |
2 |
By wall mounting, the terminal base is grounded through the screws.
-
The screws must have a conductive surface (e.g. steel zinc-plated or brass nickel-plated).
-
The mounting plate must be grounded.
-
The screws must have a good electrical contact to the mounting plate.
Practical tip
The following procedure allows you to use the mounted modules as a template for drilling holes in the panel. Due to module mounting hole tolerance, it is important to follow these procedures:
-
On a clean work surface, mount no more than 3 modules (e.g. one terminal base and two terminal units).
-
Using the mounted modules as a template, carefully mark the center of all module-mounting holes on the panel.
-
Return the mounted modules to the clean work surface, including any previously mounted modules.
-
Drill and tap the mounting holes for the screws (M4 or #8 recommended).
-
Place the modules back on the panel and check for proper hole alignment.
-
Attach the modules to the panel using the mounting screws.
If mounting more modules, mount only the last one of this group and put the others aside. This reduces remounting time during drilling and tapping of the next group.
-
Repeat the steps for all remaining modules.