With the 'Configuration of the IP settings with the IP configuration tool' a network scan can be executed, and the found devices can be assigned with new settings, e.g. enable BOOTP or DHCP and set a new fixed IP.
⮫ “Configuration of the IP settings with the IP configuration tool”
If the last byte of the IP address of the CI52x-MODTCP devices is set to 0 with the IP Configuration Tool the address switch position is used instead.