Method Ack / DiagAck: acknowledgementPermalink

This method can be used to acknowledge a diagnosis alarm previously requested by using any ‎Get...‎ / ‎DiagGet...‎ method. Alternatively, you can acknowledge an alarm in Automation Builder.

After acknowledgement, the alarm is deleted from the diagnosis system.

Scope

Name for device diagnosis

Name for device diagnosis

Type

Comment

Return

Ack

DiagAck

AC500_DiagTypes.ERROR_ID

Input

Data

Data

AC500_DiagTypes.DIAG_VAL_TYPE

Variable containing details of diagnosis alarm to be acknowledged

Example

System diagnosis: acknowledge first diagnosis message

Example_1_4_2_2_1