Menu logPermalink

When the log window has the input focus, the menu option Log appears in the menu bar instead of the items 'Extras' and 'Options'.

The menu includes the following items:

Load: An external log file *.log can be loaded and displayed using the standard file open dialog. The log that is present in the project will not be overwritten by the command. If the log window is closed and later opened again, or a new Online session is started then the version that is loaded will again be replaced by the project log.

Save: This menu item can only be selected if the project log is currently displayed. It allows an excerpt of the project log to be stored in an external file. For that, the following dialog will be displayed, in which the Online sessions to be stored can be selected:

COD_Menu_Log (AC500-S PT)

After successful selection, the standard dialog for storing a file opens ('Save Log').

Display Project Log: This command can only be selected if an external log is currently displayed. It switches the display back to the project log