Shortcut: <Ctrl>+<R>
This command inserts a RETURN instruction. Depending on the selected position, insertion takes place directly in front of the selected input (Cursor Position 2),directly after the selected output (Cursor Position 4), directly before the selected line cross (Cursor Position 5), or at the end of the network (Cursor Position 6).