'Insert' 'Jump' in LDPermalink

With this command you can insert a parallel jump in the selected LD editor, in parallel, at the end of the previous coils. If the incoming line delivers the value "On", then the jump will be executed to the indicated label.

⮫ “Coil”

The marked position must be the connection between the contacts and the coils or a coil.

⮫ “Cursor positions in the LD editors”

The jump is present with the text "???". You can click on this text and make a change in the desired label.