Shortcut: <Ctrl>+<L>
You can use this command in the LD editor to insert a coil in parallel to the previous coils.
If the marked position is a connection between the contacts and the coils, then the new coil will be inserted as the last. If the marked position is a coil, then the new coil will be inserted directly above it.
⮫ “Cursor positions in the LD editors”
The coil is given the text "???" as a default setting. You can click on this text and change it to the desired variable. For this you can also use the input assistant.
For the possibility of entering addresses, of linebreaks for variable names and of comments per coil please see the description of the Ladder Options dialog.