Automation Builder supports the connection to PLCs via hostname.
To access a PLC via hostname, the user should add the prefix “dns:” in the editor view “Communication Settings” of that PLC.
This enables a login to a PLC via hostname.
Firmware update of a PLC via Automation Builder requires the configuration of the IP-Address in bytes and will not work with any hostname.