Guidelines for creating librariesPermalink

Libraries must be created according to specific rules to avoid compatibility issues.

The main items include the following:

  • Select a meaningful library name (required)

  • Use templates to ensure consistency (optional)

  • Use a familiar and uniform project structure, when possible (optional)

  • Register a unique library namespace (required)

  • Enter all project information (required)

  • Apply the correct method for referencing other libraries correctly (required)

  • Design smart external and internal interfaces (required)

  • Implement a user-friendly error handling (required)

  • Apply the correct method (protection) for deployment (required)

  • Apply a consistent naming convention to get clean code (optional)

  • When revising an existing library, consider the interface compatibility with previous versions.

Please follow these guidelines when developing libraries in CODESYS: "Library Development Summary". You will find this document as a CHM file (LibDevSummary.chm) in the installation directory of CODESYS, or in the online help.

See also