I/O mapping export and importPermalink

Export I/O mapping

I/O mapping data can be exported as a .csv file to enable maintenance of I/O data outside Automation Builder, e.g. in MS Excel.

To export I/O mapping data, right-click the “Processor Module” node or the “I/O_Bus” node in the device tree and select “Export -> IO mapping”. To export the I/O mapping data for the entire project, e.g. when multiple processor modules are configured, select “Project -> Export -> I/O mapping”.

Import I/O mapping

A previously exported .csv file can be imported to the project: “Project -> Import -> I/O mapping”.