Shortcut: <Del>
Deletes the selected area from the editor window. This does not change the contents of the clipboard.
In the 'Object Organizer' this similarly applies to the selected object, whereby not all objects can be deleted, e.g. the PLC Configuration.
For the type of selection the same rules apply as with 'Edit' 'Cut'.
The form of the selection depends upon the respective editor:
In the text editor (ST and declarations) the selection is a list of characters.
In the FBD and LD editors the choice is a number of networks which are indicated by a dotted rectangle in the network number field.
In the 'library manager' the selection is the currently selected library name.
In order to delete a selected area and simultaneously put it on the clipboard, use the command 'Edit' 'Cut'.