Diagnosis descriptionsPermalink

Displayed text

For output of diagnosis messages in textual format Automation Builder and IEC application use text lists. Both application use the same text lists. The text lists are part of the device description. When inserting a new device in device tree of project, the corresponding text list is loaded. This text lists are part of PLC program and will be downloaded into the PLC.

Diag_V3_PLC

It is necessary to include a visualization, even if visualization will not be used. ⮫ “CODESYS Visualization”

Without visualization the text lists will not be included.

The text lists are generated automatically. We recommend that you do not change them manually because the changes can be overwritten automatically and without prompting.

Displayed text for 3rd party devices

The text lists for 3rd party devices are created during reading of the device description sheets, e.g., GSDML files for PROFINET I/O devices.

The name of a text list for a PROFINET I/O device is: Diag_PNIO_Vendor ID_Device ID

Example

CI501-PNIO: Diag_PNIO_26_22

26 = vendor ID ABB, 22 = device ID CI501-PNIO

The text list for the AC500 PROFINET I/O modules contains all text needed for PROFINET standard diagnosis and AC500 process alarm handling.

Which texts are used, depends on parameter “Selection of diagnosis method”: Double-click on a PROFINET I/O module and open tab “General”.