Project version historyPermalink

Command 'Project' 'Data Base Link' 'Project Version History

If the chosen data base system supports that functionality, you can use this command to view the version history for the currently opened project.

The dialog 'History of <data base project name>' will open. It shows the actions (create, check in, label) which have been performed for the particular objects of the project in a chronological order. The total number of objects is displayed behind Version history. The dialog can be handled like described for command 'Show Version History', but regard the following:

  • The command 'Reset Version' is only available for single objects.

  • The command 'Get latest version' means that all objects of the version of the currently marked object will be called to the local project! That means, that the objects in AC500-S Programming Tool will be overwritten with the older version. But: Local objects, which were not yet part of the project in that older version, will not be removed from the local project ! If a labeled version is called, which contains Shared Objects, then the user will get a dialog where he can decide whether those Shared Objects should be called also or not.