LoginPermalink

This command will open the dialog 'Login' where you can enter the access data for the ENI data base via the ENI Server. The access data also have to be defined in the ENI Server (ENI Admin, User Management) and – depending on the currently used data base – also in the user management of the data base. After the command has been executed, first the Login dialog for category 'Project objects' will open.

proj_db_login (AC500-S PT)

The following items are displayed:

  • Data base: project objects

  • Host: address of the computer where the ENI Server is running (must match with the entry in field 'TCP/IP address' in the project options dialog for 'Project source control').

  • Project: Name of the data base project (must match with the entry in field 'Project name' in the project options dialog for 'Project source control'/category 'Project Objects').

Credentials:

  • Insert username and password.

  • When option Use as default for this project is activated, then the above entered access data will automatically be used for any further communication between the actual project and the data base concerning objects of the actual category.

  • Press OK to confirm the settings. The dialog will be closed and automatically the Login dialog for 'Shared objects' will open. Enter the access data in the same way as described for the 'Project objects' and confirm with OK. Do the same in the third Login dialog which will be opened for category 'Compile files'.

  • The Login dialog will always open as soon as you try to access the data base before having logged in successfully as described above.

If you want to save the access data with the project, activate option 'Save ENI credentials' in the project options, category 'Load & Save'.