Creation of an archive Permalink

It is strongly recommended to create a project archive and store it separately as a backup of the project.

  1. Select “File  Project Archive  Save Archive”.

  2. Although you can select which information to include in the project archive, it is strongly recommended that you include all the information set by default.

    Do not include the “Options” in the project archive. They are not fully supported.

  3. Select [Save...] to create the archive.