|
No. |
Item to check |
Fulfilled (yes / no)? |
Comment |
|---|---|---|---|
|
1. |
Safety digital output channels from different groups (O0…O3 and O4…O7 are not in the same parallel connection. |
||
|
2. |
The DX581-S parameter “Detection” is set to “On” for all safety digital outputs connected in parallel. |
||
|
3. |
The safety application on the safety CPU controls all safety digital outputs connected in parallel with the same safety application signal. |
||
|
4. |
The safety application on the safety CPU switches off all of the safety digital outputs connected in parallel if a fault is detected on one output. |
||
|
5. |
The capacitive load per output does not exceed the following limits.
|
||
|
6. |
The current of the electrical load per safety digital output does not exceed the following limits.
|
||
|
7. |
The test pulses on the safety digital outputs (with a duration of less than 1 ms) do not affect the load. |
||
|
Reviewer(s): Machine/Application <ID>: Signature: Date: |
|||