Communication with BACnet is done through objects and properties.
The AC500 B-BC server of the figure below is represented as a BACnet device object with “ID 12”. The device contains more objects like the Analog Input object, representing the input of a temperature measurement device. An object contains several properties, like “ID, Description, Present Value, Unit” etc.
Further possible objects of an AC500 B-BC are:
-
“Binary Input” for example from connected to a switch
-
“Analog / Binary Output” for actuators
-
“Analog / Binary Values” for local variables
-
“Calender”
-
“Schedule”
-
“Trend Log”
-
...
-
A list with all details can be found in the Automation Builder pdf document ABB-B-BC-PICS-AC500_V3.pdf. Help/Project examples/.
Fig. 251: BACnet objects, properties, services and BIBBs