Addition of the VisualizationManagerPermalink

  1. add_Visualization_Manager

    Right-click “Application” in the device tree.

  2. Select “Add object”.

  3. Select “VisualizationManager”.

  4. Select [Add object] to add the VisualizationManager to the project.

    Dialog “Add Visualization Manager” opens.

  5. 01.06.02

    Select [Add].

    device_tree_visualization_objects

    You added the objects “VisualizationManager” and “VISU-TASK” to the device tree.