Using textsPermalink

You can get displayed text in an element by assigning a string in the element property “Texts  Text”. For example all base elements have this property. Also, you can get displayed a text as a tooltip (element property “Texts  Tooltip”). Texts assigned in this way are static. They are managed in the object “GlobalTextList” in view “POUs” and they cannot be modified during runtime, neither programmatically nor via an user input.

However, you can extend a static text by (exactly) 1 placeholder containing a formatting specification, in order to output the content of a variable at this place. At runtime the current value of the variable, which you have assigned to the element via property “Textvariable”, will be output.

On the possible formatting specifications please see:

By dynamic configuration you can animate the optical representation of the text.

You can localize the static texts, if you have set up multilingualism in your project.

See some examples for the text configuration of visualization elements in the following chapters.

Labeling an image element with a static text

Precondition: A project containing a visualization is opened. You have an image file representing a stop symbol.

  1. Below the Application object insert an object “Image Pool” named ‎ImagePool_A‎.

  2. In the image pool ‎ImagePool_A‎ add your stop symbol image file with ID ‎Stop‎.

    _visu_img_element_image_stop

  3. Open the visualization and from the ToolBox draw an element “Image” into the editor.

    The input assistant opens. In tab ‎Category‎ you see the image pool‎ImagePool_A‎.

  4. Select the image ‎Stop‎ and close the dialog with “OK”.

  5. Configure the property “Text” of the image: ‎ImagePool_A, Stop‎

  6. Configure the property “Text properties  Horizontal alignment”: ‎Left‎.

  7. Configure the property “Text properties  Vertical alignment”: ‎Bottom‎.

    _visu_img_element_image_stop_labeled

Text output: Element outputs the result of ST code which is executed on a mouse-click

Precondition: A project containing a visualization is opened.

  1. Open the visualization and insert a “Button” element.

    The “Properties” view opens for the new element.

  2. Configure property “Text”: ‎Number of clicks: %I‎

    The string contains the placeholder ‎%I‎.

  3. In POU ‎PLC_PRG‎ of the application declare a type-conform variable: ‎iClicks : INT;‎

  4. Configure the property “Text variable” of the button element with ‎PLC_PRG.iClicks‎.

    At runtime the variable value will be output instead of the placeholder.

  5. Below property “Inputconfiguration”, in the cell containing the input event ‎OnMouseClick‎, click on “Configure”.

  6. From the list of possible actions choose ‎Execute ST-Code‎.

  7. Enter the code for the action in the editor “Execute ST-Code”:

    ‎PLC_PRG.iClicks := PLC_PRG.iClicks + 1;‎

  8. Close the dialog with “OK”.

    The user input is configured.

  9. Build, download and start the application.

    The application is running. The visualization opens. The element is labeled and the number of clicks will be output. If you as user click on the button, the number will be increased.

    _visu_img_user_input_button

Text output: Dynamic output using a textlist

Using the “Text field” element you can produce a dynamic text output. The text output can be effected via an user input or via the application program.

Precondition: A project containing a visualization is opened.

  1. Open the visualization and insert a “Text field” element.

    The “Properties” view shows the configuration of the element.

  2. Below the application add a Text List with the following entries: ‎Textlist_A‎.

    _visu_img_textlist_a
  3. In POU ‎PLC_PRG‎ of the application declare the text variable:‎strTextID : STRING := '0';‎

  4. Also declare the variable ‎strTooltipID : STRING := '0';‎

  5. Also declare the variable ‎iText : INT;‎

  6. Configure the property “Dynamic texts  Text List” with ‎'Textlist_A'‎.

  7. Configure the property “Dynamic texts  Text index” with ‎PLC_PRG.strTextID.‎

  8. Configure the property “Dynamic texts  Tooltip index” with ‎PLC_PRG.strTooltipID.‎

  9. In POU ‎PLC_PRG‎ implement the CASE instruction as shown below.

    The variables in property “Dynamic Texts” are programmed.

  10. Configure the property “Inputconfiguration  OnMouseclick” for ‎Execute ST-Code‎ with ‎PLC_PRG.iText := (PLC_PRG.iText + 1) MOD 4;‎

    For element “Text field” an user input is configured.

  11. Build, download and start the application.

    The application is running. The visualization opens. In the text field the text ‎None‎ is output. When you as user click on the element, the text changes to ‎Dynamic_ File_A‎. And the matching tooltip is available: ‎Information A‎. With each click the text changes according to the CASE instruction.

    _visu_img_output_dynamic_text

CASE instruction

CASE iText OF 
0:	strTextID := '0';
	strToolTipID := '0';

1:	strTextID := '1';
	strToolTipID := '4';

2:	strTextID := '2';
	strToolTipID := '5';
	
3:	strTextID := '3';
	strToolTipID := '6';
ELSE	
	strTextID := '0';
	strToolTipID := '0';
END_CASE;

Text output: Configuring a static + dynamic text output

In property “Texts  Text” you can define a text in order to get a static text output. A text in “Texts  Tooltip” will be displayed as tooltip. You can configure the text in a way, that the content of a variable is additionally output.

You can extend a static text by (exactly) 1 placeholder including a formatting definition, in order to output the content of a variable at this place at runtime. The variable must be assigned in property “Text variable”. When the variable value changes in the application code, then at the same time the output in the visualization changes.

Precondition: A project containing a visualization is opened.

  1. Open the visualization and insert an element “Text field”.

    The “Properties” view shows the element configuration.

  2. Configure the property “Texte  Text”: ‎File name: %s‎

    The text contains the placeholder ‎%s‎.

  3. In POU ‎PLC_PRG‎ of the application declare a type-conform variable ‎strFileName : STRING := 'File_A';‎

  4. Configure the property “Text variable” of the text field with ‎PLC_PRG.strFileName‎.

    At runtime the variable value will be output instead of the placeholder.

  5. Build, download and start the application.

    The application is running. The visualization opens. The text field element displays the text: ‎File name: File_A‎

Configuring text input in a text field

You can use the “Text field” element in order to output the text given by a variable, or to provide a place, where the user can give input on the variable.

Additionally you can configure a text input. In this case on an user input an input field in the element “Text field” will appear. As a precondition you must have configured an user input action in the property “Inputconfiguration”.

Showing text as a tooltip

Precondition: A project containing a visualization is opened.

  1. Open the visualization and insert an element “Text field”.

    The “Properties” view shows the element configuration.

  2. Configure the property “Texts  Text”: ‎File name: %s‎

    The text contains the placeholder ‎%s‎

  3. Configure the property “Texts  Tooltip”: ‎Storage location: %s‎

  4. In POU ‎PLC_PRG‎ of the application declare a type-conform variable‎ strFileName : STRING := 'File_A';‎

  5. In POU ‎PLC_PRG‎ of the application declare also the variable ‎strFileDir : STRING := 'D:/Data';‎

  6. Configure the property “Text variable” of the text field with ‎PLC_PRG.strFileName‎.

    At runtime the variable value will be output instead of the placeholder.

  7. Configure the property “Tooltip” of the text field with ‎PLC_PRG.strFileDir‎.

  8. Build, download and start the application.

    The application is running. The visualization opens. The text field element shows the text ‎File name: File_A‎. When the mouse cursor is moved above the text field, the tooltip will be displayed: ‎Storage location : D/Data‎.

    _visu_img_output_text

Configuring element “Text field” for text input

The user should be able to enter text in a text field. For this configure an input of type “Write variable” on a text output variable. This text output variable will store the text input of the user and will display this text instead of the placeholder (this is ‎%s‎ in the example below). You specify the text output variable in the property “Text variables  Text variable”.

Precondition: A project containing a visualization is opened.

  1. In POU ‎PLC_PRG‎ of the application declare a string variable: ‎strInput : STRING;‎

  2. Open the visualization and insert an element “Text field”.

    The “Properties” view shows the configuration of the element.

  3. In property “Texts  Text” enter ‎Input: %s‎.

  4. In property “Inputconfiguration” for mouse action “OnMouseClick” click on “Configure” to open the “Input Configuration” dialog box. There choose action “Write a Variable” and activate option “Use text output variable”. Close with “OK”.

  5. In the element property “Text variables  Text variable” assign the text output variable ‎PLC_PRG.strInput‎.

  6. Build, download and start the application.

    The application is running. The visualization opens. The element outputs the text: ‎Input:‎. Click in the element to open an input field, where you can enter a string. After having terminated the input by [Enter], the text will be adopted.

    _visu_img_current_imput

Animating the text display

Configure the property “Font variables” in order to animate the display of a text. All base elements have this property, additionally the table, scrollbar and text field element.

Configuring the 'Label' element

Precondition: A project containing a visualization is opened.

  1. Open a visualization and insert an element “Label”.

    The “Properties” view with the pre-set property configuration opens.

  2. Configure the property “Texts  Text”: ‎Visualization A‎.

Making an element invisible

You can configure the property “State variables  Invisible” in order to hide an element in the visualization.

Precondition: In the visualization you have configured a text field, which gets visible only, if a certain application variable gets TRUE. For example in order to show certain instructions or descriptions only in a certain state of the machine.

  1. For the text field element configure the property “Texts  Text” with ‎Error detected: Do the following...‎.

    Configure the property “Text properties  Font color” with “dark red”.

  2. In ‎PLC_PRG‎ declare the variable ‎bIsInvisible : BOOL : TRUE;‎ (this is the initialization for the current example; normally the variable should be set to TRUE by the application program under certain conditions.

  3. Configure the property “State variables  Invisible” with ‎PLC_PRG.bIsInvisible‎.

  4. Build, download and start the application.

    The application is running. The visualization opens and the text field is not visible. When you set ‎bIsInvisible‎ to ‎TRUE‎, the textfield will be displayed.