Tab 'Visualization manager' – 'Visualizations'Permalink

Symbol: _visu_icon

Function: The tab lists all visualizations that are available project-wide and enables an assignment of the visualizations for the loading behaviour, depending on the display variants.

Tab 'Flags'

“Standard behaviour”

_cds_icon_option_activated: The visualizations of the application and the actually referenced visualizations are automatically loaded to the target system. The activated checkboxes show which one that is.

_cds_icon_option_deactivated: The loading behaviour is explicitly defined for each visualization.

Hint: use the explicit selection if you reference visualizations indirectly via IEC variables.

“Visualizations”

The list contains all created visualizations from the device tree and the POU view.

“Dialogs”

The list contains all the referenceable visualizations that are available via the libraries of the library management.