Introduction
Symbol:

Category: “Basic”
The “Polygon”, “Polyline”, and “Bézier Curve” are the same element type. They can be converted into another type by changing the “Element type” property.
Elements can be dragged to the editor. The element is then drawn with five points: [0] to [4].
Other positions are added as follows: Move the mouse pointer over a corner point; the mouse pointer changes shape. Now if you press and hold [Ctrl] and click the left mouse button, another point is created. You can delete a point by pressing and holding [Shift]+[Ctrl] and click the selected point.
As an alternative, you can select the element in the toolbox area and in the editor click multiple times. At the same time, a connecting line is drawn from one point to the other. End by double-clicking the element or right-clicking it one time.