Introduction
Symbol:

Category: “Alarm Manager”
The element is a simplified version of the alarm table. It visualizes a single alarm only. In the element properties, you specify which information is shown. You define the appearance of the element and the variables that control the element behavior.
The alarm banner displays active alarms only. If the alarm is acknowledged, then it disappears from the alarm banner.
The “Alarm Banner” visualization element cannot be inserted into a visualization in the POU pool.