Visualization EditorPermalink

The visualization editor opens when you double-click a visualization object.

_visu_img_visualization_editor
  • (1) Graphical editor: Here you create the visualization from the visualization elements which are provided in the visualization toolbox view.

  • (2) View “Visualization Toolbox”: available visualization elements

  • (3) View “Properties”: Configuration editor for the visualization element currently selected in the editor area

  • (4) Menu “Visualization”: Commands for working in the visualization editor

The “Visualization” menu contains, for example, commands for opening additional editors.

  • (5) “Interface Editor”: Declaration of variables which can be used to parameterize references of the visualization.

  • (6) “Hotkeys Configuration”: Definition of keyboard shortcuts for inputs on the visualization in online mode.

  • (7) “Element List”: List of all elements used in the visualization; possibility to change their position on the Z-axis.