Function: The dialog requests you, after changing an interface in the visualization references concerned, to re-assign the variables for the parameter transfer.
Call: The dialog appears automatically.
Requirement: You have changed the interface of a visualization, for example by adding an additional variable. After that, you have clicked either “File → Project” or “Build → Generate Code”, or you have opened a visualization.
|
“Parameters” |
Hierarchical structure of the interface parameters as a tree view |
|
Top node of the visualization hierarchy with the name of the visualization This contains an element of type “Frame” or “Tabs”. |
|
|
Name of the element (“Frame” or “Tabs” type) |
|
|
Name of the referenced visualization |
|
|
|
Interface of the referenced visualization with the new parameters You can edit the parameter transfer here. |
|
|
Interface of the referenced visualization with the previously valid parameters You cannot edit the parameter transfer, but you can use it as a template. |
|
|
Variable for the parameter transfer ( |
|
|
Variable for the parameter transfer ( |
|
“Type” |
Data type of the variable Example: |
|
“Value” |
Variable that is transferred as a parameter and with whose value the visualization is initialized during instantiation Example: If the variable lies under the current interface, which is marked in the tree view
with
|
|
“Copy” |
Link for copying an assignment from the “Value” column Requirement: An assignment is selected. |
|
“Paste” |
Link for inserting an assignment Requirement: You have copied an assignment. |
|
“OK” |
Click the button to close the dialog and confirm the changes made under “(Recent)”. Result: The assignment is entered in the “References” property and in the ⮫ “Command: Interface Editor ”. |


:
: