Dialog: Open Existing Style as Copy Permalink

Function: The dialog prompts you to specify data for copying a style file.

Call:

  • In CODESYS:

    In the editor of the “Visualization Manager” object, on the “Settings” tab, in the “Style Settings” group, click _visu_icon_activate_style_editor_cmds.png for a list box). Click “Copy and Edit Style”.

  • Visualization style editor:

    Menu: “File  Open as Copy”

“Style”

Style to be copied

Example: ‎Basic Style, 3.5.9.0‎

NOTE:

You can also select a style from the repository.

“Destination”

Working directory for style editing

“OK”

A copy of the style is created and opened for editing in the Visualization Style Editor.