Dialog: Create New Visualization Style Permalink

Symbol: _visu_icon_new_style.png

Function: The dialog prompts you to specify data for a new created style file.

Call:

  • In CODESYS:

    In the “Visualization Manager” object, on the “Settings” tab, in the “Style Settings”):

    Clicking _visu_icon_activate_style_editor_cmds.png opens a list box. Click “Create and Edit Derived Style” there.

  • Visualization style editor:

    Menu: “File  New Style”

“Name”

Name of the new style.

Example: ‎Style_CI‎

“Location”

Working directory for style editing

“Base style”

Style to base the new style on The list box contains all styles installed in the repository.

“<none>”: The new style does not derive itself from an existing style.

“Visualization Profile”

The profile is intended for informational purposes. For example, you find elements that are not preconfigured with special style entries, and information from the profile. Moreover, CODESYS checks in the profile whether a required style is missing.

Example: ‎ CODESYS V3.5 SP9 ‎

Click “OK”

The new style is created and opened for editing in the Visualization Style Editor. It already includes all required style entries and the localization in German (language column ‎de‎).