Function: The dialog lists the installed symbol libraries and allows you to assign symbol libraries to a project.
Call: “Project → Project Environment” menu, “Visualization Symbols” tab
Requirement: The open project contains a visualization and has been saved with a compiler version
less than 3.5.7.0. Symbol libraries are known in compiler version 3.5.7.0 and higher.
|
“Symbol library” |
List of all installed symbol libraries |
|
“Active” |
|
: The symbol library is selected for the project. As a result, their symbols are available
in the
: Symbol library is currently installed only in the library repository.