Dialog: Project Environment: Visualization Styles Permalink

Function: Configures the current visualization style of the project

Call: “Project  Project Environment” menu, “Visualization Styles” tab

“For the following visualization styles currently in use, newer versions are available”

“Visualization style”

Version of the set visualization style in the open project

“Current”

Current version of the visualization style (example: ‎3.5.6.0‎)

“Recommended”

Recommended version of the visualization style (example: ‎3.5.7.0‎)

“Action”

“Do not update”

The visualization style of the project remains unchanged.

“Update to x.x.x.x”

The style is updated to the specified version

“Check for updates when loading this project”

_cds_icon_option_activated_copy.png: Each time the project is opened, it checks if new versions are available. If so, then the corresponding update dialog opens automatically.

_cds_icon_option_deactivated.png: The version is not checked. The update dialogs no longer open automatically.

“Set All to Newest”

The style is updated to the newest version.