Dialog: Project Environment: Visualization Profile Permalink

Function: Configures the current visualization profile of the project

Call: “Project → Project Environment” menu, “Visualization Profile” tab

“Current visualization profile in project”

The currently set visualization profile of the open project

“Recommended, newest profile”

Newest profile

“Action”

“Do not update”

The visualization profile of the project remains unchanged.

“Update to x.x.x.x”

CODESYS updates the project to the selected visualization profile.

“Check for updates when loading this project”

_cds_icon_option_activated_copy.png: CODESYS checks for new profiles each time the project is opened. If so, then the corresponding update dialog opens automatically.

_cds_icon_option_deactivated.png: Not a test of the profile when opening the project. The update dialogs do not open automatically.

“Set All to Newest”

CODESYS updates the profile.