Dialog: Options: Visualization User Management Permalink

Symbol: _cds_icon_user_groups.png

Function: The options define the use of visualization user management for global visualizations in the “POUs” view and for visualizations that are linked from libraries.

Call: “Tools” menu

Requirement: A visualization user management exists.

Table 847: User Management Configuration for Libraries and Global Visualizations

“Do not use visualization user management”

The affected visualizations behave as when no user management is configured.

“Use the following user group list for visualization:”

  • You can edit the list.

  • The list is created in the “Visualization Manager” (“User Management  Groups”) by clicking “Export Groups for Global Visualizations”.

“Derive visualization user management automatically”

The affected visualizations use the user management configuration of the Visualization Manager selected here.

The list box shows all Visualization Managers of the project.

If this is not possible, then the user groups are used from the option “Use the following user group list for the visualization”.

The user management for a visualization in the “Devices” view is configured in the “Visualization Manager” (“User Management” tab).