Function: Creates a new object with “Visualization” type
Call: “Project Add Object Visualization”; context menu of an application
Requirement: An application is selected in the device tree.
|
“Name” |
Name of the visualization Example: |
The following settings are displayed only when you add a “Visualization” object to the project for the first time.
|
“Symbol library” |
List of all installed symbol libraries |
|
“Assigned” |
TIP: CODESYS manages this setting in the project settings. |
|
“Add” |
Creates the new visualization and assigns the selected symbol libraries to the project. These are available in the “Visualization Toolbox” view. |
: Symbol library is selected